AXIS#.WS.CHECKV

Description

This parameter sets the velocity threshold which has to be exceeded to activate commutation monitoring.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

N/A

Data Type

Float
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
AXIS1.WS.CHECKV

5013h

0bh

Signed32

Velocity

-

Read/Write

No

AXIS2.WS.CHECKV

5113h

0bh

Signed32

Velocity

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.WS.CHECKV

6716

1A3C

Signed32

Read/Write

Velocity

AXIS2.WS.CHECKV

72252

11A3

Signed32

Read/Write

Velocity

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.WS.CHECKV

6716

Float

Read/Write

Velocity